Use the Group function to "group" identical N6700 power modules that are connected in parallel. This will configure the designated channels to act as a single channel, allowing commands to be sent to only one channel in the group.
Refer to chapter 4 under “Output Groups” in the N6700 User’s Guide for further details.
http://literature.cdn.keysight.com/litweb/pdf/5969-2937.pdf
Refer to chapter 6 under “Output Grouping” in the N6705 User’s Guide for further details.
http://literature.cdn.keysight.com/litweb/pdf/N6705-90001.pdf
When using SCPI for example, simple send the following commands to configure the group function. This allows you to send subsequent commands to channel 1 only:
SYSTem:GROUp:DEFine (@1,2,3) followed by SYSTem:REBoot.
Refer to the Group command in the Programmer’s Reference Guide.
http://literature.cdn.keysight.com/litweb/pdf/N6700-90902.pdf.
N6700A, N6700B, N6701A, N6702A, N6705A, N6705B, N6710B, N6711A, N6712A, N6715A, N6715B, N6731B, N6732B, N6733B, N6734B, N6735B, N6736B, N6741B, N6742B, N6743B, N6744B, N6745B, N6746B, N6773A, N6774A, N6775A, N6776A, N6777A, N6751A, N6752A, N6753A, N6754A, N6755A, N6756A, N6761A, N6762A, N6763A, N6764A, N6765A, N6766A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |